Hi All,
I have been using digi zigbee for a while and I use pic32 to send/ recieve data. I never though about ti cc2530 chip to include in my design and this will allow me to make single board instead of 2 boards. I can see cc2530 is MCU itself and I really didn't need to have pic32 to send data. I could of done everything is single ic such as cc2530. since I am really new to Ti cc2530 in my case I just want to load a some kind of test code that has fallowing feature. 1. RX, TX
2. data encryption over RX, TX
3. security to block reading back
4. is this single point to point communication? or mesh? or that's all in software what to do?
5. do I need to use can box to cover the cc2530 or do not need
6. can I use on board F antenna to send about 100 feet range
thanks
everything else is not used at the moment
my question is where can I get the test code to start using it until I learn more about it.
any info will appreciate.
Andre