hello,
I have a zigbee cc2530 module connected to its cc2530 baseboard and the baseboard is connected to the pc via usb cable ..on the other side i have an arduino connected to xbee pro s2 module via xbee shield...the arduino is powered by a battery ..can i achieve wireless communication between the cc2530 module and the xbee on the arduino? if yes how to do that?
thank you