This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Firmware Library and Examples Rev.B released

Other Parts Discussed in Thread: CC2511, CC2531, SIMPLICITI, CC1111EMK868-915

 

Our USB Firmware Library with software examples has been updated to Revision B. The new release features:

  • Supports CC1111, CC2511 and CC2531
  • HID example emulates simple mouse and keyboard operations using a SmartRF04EB or SmartRF05EB
  • CDC example with RF Modem/Virtual UART
  • MRFI radio link layer (MRFI is the link layer used by SimpliciTI)
  • SW tested against USB Command Verifier, passing Chapter 9 and HID tests (the USB Command Verifier is a part of the USB certification process)
  • HID and RF Modem SW examples rewritten from scratch
  • Documentation split in software and hardware manuals
  • Tested on Windows XP SP2/SP3, Windows Vista SP1 and GNU/Linux (Ubuntu 9.04)
  • Bug fixes to the USB Firmware Library, CDC class and HID class

 

The software and the documentation can be downloaded from the following web pages:

  • http://focus.ti.com/docs/toolsw/folders/print/cc2530dk.html
  • http://focus.ti.com/docs/toolsw/folders/print/cc2511emk.html
  • http://focus.ti.com/docs/toolsw/folders/print/cc1111emk868-915.html