Other Parts Discussed in Thread: Z-STACK
Hi all,
I am using zstack home 1.1.0 and trial version of IAR WB 8.20
i am getting a lot of errors while compiling the code. the same code works fine the previous evening and next day morning, i see a lot of errors.
today i installed IAR WB 8.3 trial version. and now i find that the previously working code ( compiled with v8.20) is giving me the following errors.
""Error[e46]: Undefined external "?V12" referred in AF ( E:\BetaBackup - heartBeat\ZC_bc_7_SWStatusAtRestart_Redo\ ""
did anyone got these type of errors earlier?
why am i getting these errors? this is a compiled and working code till morning. now i am getting these type of errors from ?V1 to ?V15.
Pl. help me in solving these errors. i compared the project options of both IAR v8.2 and v8.3. they are same. then what could be the problem?
Thanks in advance ,
Mahesh KV