Hello
I am a student of University of the Aegean . As part of my thesis I use cc2530ZDK , and I have some questions about cc2530zdk I wanted to ask you. Initially I want to describe what I want to achieve and ask your advice . My aim is to study the energy efficiency as a function of link quality first for the pre -programmed sensors and then making my own scenarios . My first thought is to create the network and instead of connecting it to the ZSensor Monitor, to connect it to SmartRF Studio setting the gateway as receiver to get packages with the corresponding RSSI and total PER (%). What I get as a result, but I do not know if it's right, because I noticed large PER and packages that I couldn’t understand the information about temperature (temp) and voltage. That’s why I would like to ask you if the procedure I am following is correct or the connection with the SmartRF Studio cancels my default network and impose another condition?. If so , how do I get the data I need ?Is there any way that you can suggest me ?