Dear TI Employee
Recently I went through the TI’s Application Report (SWRA427B–November 2013) by Suyash Jain titled “Breaking the 400-Node ZigBee® Network Barrier With TI’s ZigBee SoC and Z-Stack™ Software.”
Section 4 of this document throws light on the Z-Stack Settings( like NWK_MAX_DEVICE_LIST ,LINK_DOWN_TRIGGER, NWK_ROUTE_AGE_LIMIT, BCAST_DELIVERY_TIME, ROUTE_DISCOVERY_TIME, NWK_LINK_ STATUS_PERIOD etc.) for the large network but limited to 4 hops. I would request Suyash (or any other TI employee who can support) about the settings that need modification(along with the optimum value) when the network is as follows:
1) 25 nodes
2) placed on ground
3) In a straight line at 25 mtr distance one after other(transmitting at 5dbm).
4) 4 nodes(of the 25 nodes) sending data every 120ms( 85 bytes as payload) and all 25 sending 10 bytes as payload every 5 seconds.
5) So probably having 25 hops in a worst case.
Please consider this as really important.