This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SampleApp ZStack 1.4.3 with CC2430 message transmission problem

Other Parts Discussed in Thread: Z-STACK, CC2430

Greeting everyone, I am new to this forum. During my development on creating a WSN with CC2430 I encountered a problem. The WSN is composed of one enddevice and one coordinator, a RFID reader is connected to the end device via uart0 which I can read the ID from the RFID reader without problem, but when I try to transmit the ID via the SampleApp_SendFlashMessage() I cannot be sure it can success everytime. I know that the network condition may not be perfect, and it would miss packets, but I receive no error message using the if (DataRequest)...else (). Nothing in the else statement is executed when I see that coordinater can't receive the message via a RS232 printout. I am not sure about one thing : Is my message successfully sent? If not, are there any place in the stack I can be informed of the transmission error, so I can resend, or redone? Thanks you guys, I already dig up the datasheets, and Z-stack manuals, but couldn't find the answer. Best Regards, Rimusuki_Korusakofu