This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2480 default Tx power

Other Parts Discussed in Thread: CC2430, Z-STACK, CC2530

Hi,

My question relates to a previous post on this forum which was never clarified.

The CC2480 has RF test modes which can be enabled via the SYS_TEST_RF command. I've implemented the API function to enabled these and it works, however I need to set the TxPower parameter to match the same power level as per the normal operating mode. It's a requirement for compliance testing of a product.

I would like to know the default Tx power level for the CC2480 under normal operating conditions. Unfortunately I was unable to find this documented anywhere.

Here is the list of settings for SYS_TEST_RF:

TxPower

Output power [dBm]

0xFF

0.6

0xDF

0.5

0xBF

0.3

0x9F

0.2

0x7F

-0.1

0x5F

-0.4

0x3F

-0.9

0x1F

-1.5

0x1B

-2.7

0x17

-4.0

0x13

-5.7

0x0F

-7.9

0x0B

-10.8

0x07

-15.4

0x06

-18.6

0x03

-25.2

Any help would be greatly appreciated.