Hi,
I am working on a CC2530+CC2591 based Zigbee solution and I am confused about LQI and RSSI values I am getting.
According to the design note below a low value indicates a better link than what a high value does.
http://e2e.ti.com/support/low_power_rf/w/design_notes/calculation-and-usage-of-lqi-and-rssi.aspx
But during my experiment I found that I was getting a higher LQI values when my modules where closer and it was reducing as I moved them far.
When both the modules where closed I got an LQI value of D9 (using Z-tool) and the RSSI value around -20dBm(using smartRF studio).
And when both the modules where around 300m far I got an LQI value of 4 and an RSSI value of -83dBm and the packet loss percentage was 3%.
Since the packet loss percentage is as low as 3 percentage I consider it to be a good link but the LQI values are confusing me.
Please help me on this.
Thanks
JK