This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuration problem, more than one routers.

Hello everyone, I'm Alejandro Rivera from Chile. I'm currently working in a project with ZigBee 2006 and ZStack-1.4.3-1.2.1.

I have a problem and maybe someone can help me out, the thing is that I've modified the SerialApp to make an App of my own. The problem is when I try to connect more than one Routers in the network, because I start the first one and the coordinator give to that device the 0x0001 address and when I start the second router the coordinator give the same address to that one.

I thought that  the network didn't support mesh topology but I've checked the nwk_globals.h file and the STACK_PROFILE_ID is set to HOME_CONTROLS, so it should be mesh.

Does anyone have an idea of what can be the problem?

Thanks!

 

Alejandro Rivera