Other Parts Discussed in Thread: CC2530
Folks,
I have done range profiling using smartrf Board with cc2530 and Antenova Antenna. Theoretically Zigbee will Communicate up to 90 meter in Line of Sight. But I am getting just 23-30 meter. The i profiled with Two Concrete Wall, it is not exceeding more than 5 meters and then with Two wooden Wall, it is given 6 meter. Typically for two Concrete it should communicate up to 30 meter. What will be the Problem? Is the Problem with Antenna?