Other Parts Discussed in Thread: CC2530, MSP430F5438, CC2530EMK
do we need any launch pad for interfacing msp430 and cc2530
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2530, MSP430F5438, CC2530EMK
do we need any launch pad for interfacing msp430 and cc2530
i am using MSP430F5438 and cc2530EMK. No, im not asking for ZAP and ZNP interfacing. i want sample codes for this
There is no such example. I would suggest you to use UART as interface between MSP430 and CC2530 in your case.
thanks for your reply.,
can i program the CC2530 EMK with EM Adapter booster pack., and i've the CC2530 and 5438 boards. the EMk of 2530 supports only SPI protocol. So i cant use the uart protocol for communication.
can i get any sample code for 2530+5438 in CCS compiler rather than the IAR.
thank u
can i get sample codes for SmartRF05EB and can u please send me the formal quotation for SmartRF05EB to forward it to our head of the department to get this board.
Hi,
I am not TI employee and don't sell SmartRF05EB to you. To get the quotation, you can go to TI eStore at https://estore.ti.com/CC2540DK-CC2540-Development-Kit-P2622.aspx
SmartEF05EB is used for download FW, debugging, or IO extender. There is no example code for it.
Hi Prasanna,
An option for programming the CC2530 is a CCDebugger.
Cheers,
Fredrik