Hey everyone!
I have a problem with the minimum idle time between ZLL-commands in Multi- and Broadcast.
We are developing an App for an Android device to control our ZLL-Lamps. If the user changes (e.g.) the level with the corresponding slider, a command is send every 100ms to change the level of the selected group.
The problem: After a few transferred commands the lamp stops to change the level for a short time, but then the lamp reacts normal. This behavior is repeated, until no commands are sent.
If we change the idle time to about 350ms everything is working perfect, but there is a to big time offset between the App-Level (nominal value) and the Lamp-Level (actual value). We want to reduce this idle time to 150-200ms, because it does not look good.
Thanks in advance!
best regards
Mario