Other Parts Discussed in Thread: CC2530
Hello
For the code given below
#if defined MT_TASK
#define HAL_UART_ISR_TX_MAX MT_UART_DEFAULT_MAX_TX_BUFF
#define HAL_UART_ISR_RX_MAX MT_UART_DEFAULT_MAX_RX_BUFF
#define HAL_UART_ISR_HIGH MT_UART_DEFAULT_THRESHOLD
#define HAL_UART_ISR_IDLE (MT_UART_DEFAULT_IDLE_TIMEOUT * HAL_UART_MSECS_TO_TICKS)
#else
#if !defined HAL_UART_ISR_RX_MAX
#define HAL_UART_ISR_RX_MAX 128
#endif
#if !defined HAL_UART_ISR_TX_MAX
#define HAL_UART_ISR_TX_MAX HAL_UART_ISR_RX_MAX
#endif
#if !defined HAL_UART_ISR_HIGH
#define HAL_UART_ISR_HIGH (HAL_UART_ISR_RX_MAX / 2 - 16)
#endif
#if !defined HAL_UART_ISR_IDLE
#define HAL_UART_ISR_IDLE (6 * HAL_UART_MSECS_TO_TICKS)
#endif
#endif
May I know the exact meaning and its usage in UART - CC2530