CC2530
1.What is the Debugging interface,since it doesn't have JTAG.
2. What is the console interface, UART?
3.What is the flashing interface, USB or UART?
CC2538
same three question for CC2538
4. I could not able to see in the which pin is for UART2(UART1 is in Port A), I2C, SPI. In the Data sheet it is mentioned that it has 2 UART, 2SPI and 1 I2C. But where is in the pin diagram