Other Parts Discussed in Thread: CC2530, CC2538, Z-STACK
Hi,
I've read the 'Breaking the 400 Node barrier' pdf and it gave me some good insights about source routing and many to one routing. The part about APS ACK was especially interesting to me - it should increase reliability of the concentrator to the routers.
If I understand correctly, enabling APS ACK would require the concentrator to (ideally) have a route in memory for each router. In the pdf there's talk about a concentrator 'with' memory, meaning that it has more memory than the standard CC2530, is that right? It's implicit from the possibility to set a flag saying there's no memory constraint...
How would I go about adding RAM to an existing CC2530, it seems impossible. Maybe I need another device for my concentrator? Or maybe use an external flash?
I'm very interested in your opinion about this.
Regards,
Sjef.