Hello
I want allocate a block of flash put the user define data in end device(not use osal nv function), current code space define (Zstack 2.5.1)use page from page 0 ~ page 120, how can I change the code space define from page 0 ~ page 100, then I can use the page 101 from 120.
If I use current define, I can write data into page 100, but I can not erase this page, so I think may be it has some relation about code area define.
Thanks