Hello,
I am currently working on a project where I have a static wireless module (maybe the cc2530) and a moving modules it's speed is about 60mph to 70mph and it's about 500m away from the static module.
I want to know if the cc2530 can work for this application. I need to transfer about 10-50bits of data to the moving module as it passes by. Do you think this can work with zigbeepro?
The thing is we have alot of these cc2530 development kits so we rather use them if they can work. Also what module would you recommend?