Other Parts Discussed in Thread: CC2530, CC2531, CC2511
I'm using a 2450BM15A0002 with a CC2530 and i having some problems with the impedence of the stripline. I know that the output impedance of the CC2530 is 69+j29 and that the balund match the impedace with a unbalanced output at 50 ohm. But what is the phi of the balun ? Maybe the output impedace is 50+j0 ? I can't understand it from the datasheet.