Other Parts Discussed in Thread: CC2530, Z-STACK, CC2538, CC2531
Hi,
My idea is to add the over the air functionality to my apps based on Z-Stack Home 1.2.0 that include CC2530 and CC2538 HW plaftorms. After reading some post I found:
OAD: ZigBee public profile for image upgrade over the air.
OTA:TI proprietary profile for image upgrade over the air. Obsolete?
My apps dont use any ZigBee public profile and the idea is to select one of those options to develop a propietary OAD/OTA funcionality. I have seen on the example that OTA is supported for CC2530 and CC2538, but OAD is supported for CC2538 too? -The documentation about OAD is too old and there is no information about that.
Another question is, does the CC2538 support the external memory to store the downloaded image? Any example or guide?
I hope somebody can help me with the right choice of the best option to develop the OAD/OTa funcionality. Any information about the steps to follow to achieve this would be appreciated.
Thanks in advance to everybody!