Hello,
I want my End Device to sleep when Ever there is no operation to perform. I have seen the Document provided by Zstack. That we need to enable the Compile time option POWER_SAVING. The Default Sample Light for End Device is xPOWER_SAVINGS What does it mean.
And in that document, setting the poll rate also is important, which will affect the Timer Sleep. DPOLL_RATE = 1000. It is recommended to increase the poll rate to 5000(500 millisecond). DPOLL_RATE is the periodic poling for Coordiantor for Queue(to check any data is available or not). Then,
What is -DQUEUED_POLL_RATE?
What is DRESPONSE_POLL_RATE?
Is there any other option for power saving.