Hi,
I installed smartRF05 packet sniffer, so along with that driver for CC2531 got installed. I also used packet sniffer for few days.
Yesterday, I tried flashing a sample application in CC2531 with CC Debugger. When I clicked on Download and Debug, I got two choice of device: CC Debugger and CC2531, when I clicked on CC2531 it gave fatal error: Unknown exception in driver. So I selected CC Debugger after that and it was downloaded and verified successfully. But after that my machine stopped detecting CC2531 USB dongle with error: " The last USB device you connected to this computer malfunctioned and Windows does not recognize it " and the device status in device manager reads "Windows has stopped this device because it has reported problems (Code 43)"