Other Parts Discussed in Thread: CC2531, CC2541
I have look at many reference designs for your PCB antennas. While I'd like to copy as close as possible, I generally find that I need to move the uC a little farther away or I need to flip the antenna. In either case I find myself computing the trace width to keep a 50ohm impedence match (may not even be saying this correctly). What I have never really understood is where that begins and ends. For instance, looking at the CC2531 USB dongle design, the trace is wide all the way to the balum. I see many designs from other vendors where traces between the device that make up the matching network are as small as 4mil. Are the trace widths in this area critical? Assuming no balum, where do the trace widths matter? My assumption has always been that the traces from the uC to the first devices were thin and from there I would make them as near as possible to the computed value using impedance matching software.
Cheers