In CC253x user guide , page 79 the following statements are confusing. Does it mean that when no internal pull-up or pull-down is configured. All the ports need to be pull up or down specifically?
7.1 Unused I/O Pins
Unused I/O pins should have a defined level and not be left floating. One way to do this is to leave the pin
unconnected and configure the pin as a general-purpose I/O input with pullup resistor. This is also the
state of all pins during and after reset (except P1.0 and P1.1, which do not have pullup or pulldown
capability). Alternatively, the pin can be configured as a general-purpose I/O output. In either case, the pin
should not be connected directly to VDD or GND, in order to avoid excessive power consumption
Thanks in Advance
Adarsh