Hi,
I have a coordinator and two end device, now I have connected the cordinator and two end device with EZ mode, but the problem is that coordinator sends the same message to the two end diveces. So I need to identify the divices and only send the message to one device.
I've been thinking in to get extended address or short address of each device, but i dont know what is the best way and how can i do that.
Also, I think that maybe I identify each device with short address but the same problem, i dont konw how can I set short address for each device.
Could you help me with this please? Any idea?
Thanks for your help.
Best regards.