Other Parts Discussed in Thread: CC2538
Can the CC2538 RESET_N input be left floating?
The evaluation module has it connected to an RC low-pass (2.2K/1nF), but when the board is standalone, it is essentially floating. The datasheet and the user guide doesn't specify if this pin has an internal pull-up.
If it is not needed, what is the recommended way of terminating it?
thanks,