Other Parts Discussed in Thread: CC2530EM, CC2530
Hi ,
I'm using the CC2530EM board, the firmware flashed is unknown but I'm measuring a 0.7V on certain GPIOs, and I would like to understand or guess in which state are this pins? I tried to pull down this GPIOs with a 2.2Mohm resistor but still stay on 0.7V so I guess the output drives and is not a floating state.
The EM goes on a motherboard that we are working on, our firmware set the pins correctly but between the moment of plugging the EM , the CC debugger and flashing the CC2530 , this 0.7V level on this GPIOs drives some of the hardware that we designed in an unwanted way and curiously goes up to 2V . So understanding this state will help us design correctly our driver and make it immunized properly.
Thanks in advance for your answers.
Amjad