Hello,
In my project I want to test 6LoWPAN connectivity with CC2538 design kit.
Here is a nice example on the following page (adopted for Atmel):
http://contiki.sourceforge.net/docs/2.6/a01789.html
At the bottom I've put a diagram from this setup.
My question is can CC2531 dongle (part of CC2538 DK) fulfil the same as RZ USB stick from Atmel, i.e. serve as bridge between CC2538 and PC ?
I've tried to proceed in the same way as described in this Contiki manual, but CC2531 isn't seen at PC: executing of
"netsh interface ipv6 show interfaces" (windows 7 version of "ipv6 if", presented in manual (used in Windows XP))
gives the same results either CC2531 is plugged or not.
Thanks in adavnce
Pavel.