I am having problem with binding and targeting a specific node among multiple similar nodes.
1. In EZ-mode binding, as far as I understand, both of the devices that are to be bound, have to be interacted with by a key press, or some other way. But I need to make a binding entry between two nodes/endpoints where one of the nodes can not be interacted with, it can be accessed only OTA(over the air). How can it be done?
2. If I have multiple devices of the same type, say, 4 lights and I need to control the lights individually a single controller end point/node, how can I do it?