Hi,
in the TIMAC stack it is given that the system clock is 12 MHZ and the SPI clock is 6 MHZ.
i want to know whether we can increase or decrease the SPI clock for given 12 MHZ system clock,
if yes can you suggest me a way of doing so .
thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
in the TIMAC stack it is given that the system clock is 12 MHZ and the SPI clock is 6 MHZ.
i want to know whether we can increase or decrease the SPI clock for given 12 MHZ system clock,
if yes can you suggest me a way of doing so .
thank you.
Pratap,
The CC2520 is a slave device and is specified to work at any SPI clock rate up to 8MHz.
Please see page 33 on:
http://www.ti.com/lit/ds/symlink/cc2520.pdf
Regards,
/TA