Other Parts Discussed in Thread: MSP430F5438, Z-STACK
Just now i am using Anaren A2530E24C chip with AIR-ZNP firmware (ZNP stack) which is communicate with MSP430F5310 via spi. Anaren chip has ZNP spi stack. But i want Z stack for developing zigbee home automation profile to interface with MSP430 via SPI not via uart. As I want to control zigbee based devices using home automation profile from our coordinator.
As i have download source code of home automation from this path C:\Texas Instruments\Z stack Home 1.2.1\projects\zstack\ where so many file is found, but same file available is supported with MSP430 or not reply
now sugest me steps as i have to operate thermostat device using home automation so which header files & c file i will be use for creating projects with msp430F5410 .
And Anaren A2530E24C chip with AIR-ZNP firmware loaded is support for home automation or another exe has to be load for supporting home automation