Hello All,
i am working on some zigbee project and i got some doubts. if anyone can help me to solve this then it will be very helpful for me.
my doubts are -
1) from zstack-home developers guide i understand that we can add our own custom attribute in a project as per our need. but can we implement and add our own custom clusters in a home automation profile ? if yes then plz tell me what is the procedure or steps to do that? i dint want to implement private profile...i just want to implement and add my own custom cluster in existing HA profile that's it.....
2) can two application profile is possible in a same same device or on a same endpoint simultaneously? if yes then plz tell me what is the procedure or steps to do that?
3) if suppose i hav 2 ZED and 1 ZC out of that 2 ZED one is having HA profile and other is having SE profile then is this possible to bind and communicate between both ZED via ZC... i mean to say is this possible that ZC can route/send/receive msg from HA ZED to SE ZED and vice versa ? if yes then plz tell me what is the procedure or steps to do that?
plz anyone help me to clear this doubt...
Thanks & Regards,
Maneesh Singh