I just trying the new Z-Stack Home 1.2.1. Compile the samplelight and flash on CC2530EM. Run it normally but the LCD Display is blank. Why is that? When using Z-Stack Home 1.2.0 all is ok. compile option is almost the same except there is additional compile option in new Z-Stack Home 1.2.1. No changes being made. There is LCD_SUPPORTED=DEBUG in compile option.
Hardware:
SmartRF05 Rev 1.8.1, CC2530EM.
Thanks.