This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After OTA upgrade cannot connect to TI Gateway

Other Parts Discussed in Thread: CC2530EM, Z-STACK, CC2530, CC2531

Using Z-Stack HA 1.2.1 & TI CC2530EM with SmartRF05 v1.8.1 on samplelight. I name it version 1.
I add OTA feature on samplelight. Merge Boot.hex and SampleLight.hex and flash into CC2530 as ZED.

Another CC2530+SmartRF05 running as Dongle.

Everything is working. SampleLight can control using physical button SW1 and can connect to TI Gateway(Beaglebone+CC2531)
Now I test the OTA feature. Compile same SampleLight as version 2. No code changes.

Run OTA Server v2.0.7. select new .zigbee file. open dongle, and ZED is detected. I run image notify and it start downloading new image.
When complete, ZED disappear and reappear again.(Hold AutoStart is disable).

Tested again, this time SampleLight can control using physical button SW1 but cannot connect to TI Gateway(Beaglebone+CC2531). Tried on/off and enable permit join many times.
No luck. Any advice?

Thank you.