Hi all,
I have to implement a HA coordinator for controlling endpoints (On/Off actuators) inside home automation environments. The hardware consists of an Anaren module (CC2530 inside) and a 8051 / 64K flash / 8K ram controller.
The endpoints use Telegesis modules with the HA1.1 profile implemented.
Is it possible to use Anaren's AIR-ZNP firmware or would it be better to flash the modules with the Z-stack HA firmware?
What would be the best starting point to embed the coordinator functionality onto the 8051 (firmware examples to port from) ?
Best regards,
Rolf