Other Parts Discussed in Thread: CC2591, CC2530, Z-STACK
I wonder what is practical range of CC2531-CC2530(with CC2591) indoor? It's said in datasheet can support up to 1000m outdoor, CC2530(without CC2591) 100m outdoor. As I test it roughly around 17m range only. More than that it's ittermittently connect/disconnect with coordinator. CC2530(without CC2591) much worst, might be 5m for stable range.
This is star topology, coordinator to many Endpoint(samplelight).
Then I extend it much further using Coordinator-many Router(samplelight)-many Endpoint(samplelight). This is mesh network right? Seem that I can extend the network further this way. Unfortunately, reconnection router/endpoint to coordinator took really much more time(1-2minutes). Sometimes it's failed to connect/disconnect by itself. Turn On/Off light also had a delay. Sometimes no response due to disconnection.
There is just release TI Z-Mesh stack, if I want to use this integrate to HA stack. How can I proceed? Will it give some improvement to the network?
For normal 2 storey house with around 20 lights/devices, should I go star or mesh? What topology would you all recommend? For mesh, how many routers/endpoint should there be for 20 lights?
Thanks