Other Parts Discussed in Thread: CC2530
Hello, i have problem with configuring my parameters using ZB_WRITE_CONFIGURATION command.
i am using ZNP CC2530 ZStack, i connect the cc2530 to an external 8051 uc through SPI interface, everything is working fine, i get all expected bytes from CC2530, but i have found that nothing of the parameters i changed by explicitly is really changed. for example i would like to change the ZCD_NV_STARTUP_OPTION to be 3 instead od default value 0, i get all the message that tells me the command is success, bu t when i try to read the value after i reset i found it unchanged. what seems to be the problem???