I used selfmade board with CC2530. Version of Z-Stack - 2.5.1. Work with ported SampleApp and ported HAL for my board (without changes). Porting made with HAL Porting Guide
I tried change pin assigments of LEDs and keys and have problem.
For example, I change in hal_board_cfg.h default HAL_LED_3 defined as
#define LED3_BV BV(4) #define LED3_SBIT P1_4 #define LED3_DDR P1DIR #define LED3_POLARITY ACTIVE_LOW
to
#define LED3_BV BV(0) #define LED3_SBIT P2_0 #define LED3_DDR P2DIR #define LED3_POLARITY ACTIVE_LOW
and it doesn't work - I can't change state of theese LED.(PUSH2_SBIT, whick on default equal to P2_0 is changed)
Because I have a question - how I can and how I have to change pin assigments (LEDs, keys)?