This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which pin of Anaren A2530E24C is used for loading hex code

Dear All,

                    I have to load hex file of stack to Anaren chip A2530E24C but i don't know which pin is used for loading code, reply which pin of Anaren chip is used to load the code.

  • You can refer to page 21 of A2530E24C user manual at http://www.anaren.com/sites/default/files/user-manuals/A2530E24x_Users_Manual.pdf and do the following connections:

    • Pin 1 of CC debugger to GND
    • Pin 2 on CC debugger to VDD
    • Pin 3 on CC debugger to DC, i.e. P2.2
    • Pin 4 on CC debugger to DD, i.e. P2.1
    • Pin 7 on CC debugger to RESETn