Other Parts Discussed in Thread: CC2538, Z-STACK
Hi,
Can any one answer my below questions.
1. I have C2538dk with SmartRF06 Evaluation board. What is the default OS it comes with?
2. If there is no default OS, then how the examples(PER test, Zigbee stack test) given in TI websilte are working. Are there any OS files or libraries included in the given IAR workbench.
3. If there is no default OS, then how to flash OS onto C2538dk. I have seen examples where the application is compiled along with Contiki source code and the resulting binary is flashed to CC2538. Instead i want to flash contiki OS first on CC2538 and then flash only standalone applications on top of contiki. Is it possible?
Thank you,
Chandrakala