Other Parts Discussed in Thread: CC2591, CC2520, MSP430F5437A, Z-STACK, CC2530
Hi All
I am new at this. I am working with the LSR ProFLEX01-R2 (which uses MSP430F5437A + CC2520 & CC2591) and I want to load the needed firmware to use the standard ZigBee. How can I load the firmware to be able to use the standard ZigBee with the PorFlex01-R2? Where can I find the needed firmware?
I would also like to know the communication protocol, i.e, the format of the frames to comunicate with modules and the configuration to setup the modules as a coordinator, router or end device.
Thank you.
Best regards,
Paula.