Other Parts Discussed in Thread: CC2530
Hello,
I have a question regarding UART on CC2530. My CC2530 is powered from VCC = 3V but I was wondering if I can "setup" the UART to work at 1.8 V because I have another device what uses 1.8 V UART. I was wondering if this is possible considering the power from CC2530 is internally regulated to 1.8 V:
(The digital core and peripherals are powered by a 1.8-V low-dropout voltage regulator (Chapter 25).) from CC253x Userguide.
Thanks,
Mircea