Other Parts Discussed in Thread: CC2530, CC2538
now i want to create the simple project for CC2530 by using contiki os .pls anyone help me .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Karthi,
Use the following TI E2E forum for your CC2530 queries.
Hi karthi,
I am moving you post to Wireless Connectivity Forums where in the queries on CC2530 have being addressed.
Regards,
Shankari
Hi Karthi,
As I mentioned in the other thread where you asked the same question: please have a look at the Contiki wiki page: http://processors.wiki.ti.com/index.php/Getting_started_with_Contiki_and_CC2530
Cheers,
Fredrik
Hi Jonas,
I had gone throught the /examples/cc2530dk directory, github.com/.../8051-Based-Platforms and the Contiki github wiki too, I find the codes there difficult to understand since i am a beginner. I have a cc2530 custom pcb, so using cc2538 is not an option for me, sadly. I have an NXP lpc1347 custom board on which a radio board(with cc2530 mcu) and a sensor are mounted. I just wanted to check the communication between 2 such setups. Basically i wanted to check whether the Contiki cc2530 examples send the recieved packets (via rf) to some target (either SmartRF05eb or Computer interface) via UART after truncating the protocol headers. Also, I have a TI cc debugger which i am using to flash my custom cc2530 pcb, my question is: if I use IAR, will i be able to debug the program? Go line by line to understand what is happening?
Regards,
Kabir