I probe RF pins of a CC2538EM.
Here is the output when it is in idle state.
Then I get the below output when I set the MCU to transmit 0x5 via RF Studio:
while I have this settings:
I think it is obvious that glitch look like signal is the data signal to be transmitted. What is the square wave that oscillates with 1.36 Hz?