I am a beginner here. I am working on an application ( like STAR network ) using Sample Switch application as a Zigbee Coordinator and Sample Light application on more than one Zigbee Routers. I want to control the light ( on/off ) on a single router amongst the many routers in the network. But after the invocation of EZ-mode the ( on/off state ) light on all the routers are changing their states after sending the command from the coordinator. How to resolve this issue?
Is address based packet filtering already enabled in this stack? If so how can I use unicast?