Other Parts Discussed in Thread: CC2538
According to the data sheets the current consumption of the CC2538 is about 24 mA with the transmitter @ 0 dBm. I have a custom board, and I measured the current consumption of 44 mA with the transmitter @ 0 dBm. Going into mode 2 deep sleep mode the current consumption is 0.6 mA, therefore I don't believe the other components are contributing to this. Also when I made the measurement of 44 mA just about all the peripherals were inactive. Could anyone offer an explanation of this 20 mA extra current?