Other Parts Discussed in Thread: CC2538
I am following the AN068 for CC2538EM, but I can't get the impedance matching. I would appreciate if someone can tell me what I am missing.
According to the datasheet, the optimum load is 66 + j64 ohm at RF_P and RF_N. Referring the Figure 7 of the App note (below):
I should have the source part as 33 + j32 ohm and the load should be 16.5 + j0 ohm.
The copper length from RF_P to L373 (RF pin to sum point of the balun) is approximately 2.564 mm. The copper width is 0.15 mm, copper thickness 35 um, dielectric thickness to the layer 2 (ground plane) is 0.175 mm. The app note suggests to use 4.1 as dielectric constant, 0.0155 loss tanget. I add those values into NI's line calculator which outputs impedance as 72.6885 and electrical length as 12.6265 degree
The schematics of CC2538EM uses 2 nH and 1 pF for the balun network.
I add the values to a Smith Chart as the chapter 6 of the App note does.
step 1: I added the load as 16.5 + j0 ohm (the red circle) and source as 33 + j32 ohm (blue circle)
step 2: I add a 2 nH serial inductor and 1 pF shunt capacitor, and then the transmission line with 73.9 ohm and 12 degree (closest possible values on the smith chart program that I use)
As you can see below, source and load is not matched. Do I miss anything on the above calculation or to follow the app note?