This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Huge delay happens on end device when it receives message CC2538

Hi friends,

I am a student working on a project based on sample temperature sensor. The wireless communication between coordinator and end device has some problem: when I use zcl_SendReportCmd from coordinator to end device, it takes seconds for end device to receive the message, which is so strange. But when I use the same function from end device, coordinator gets the message immediately. I have kept the end device in PM0 mode.

What is the problem?

Regards,

Jay