Other Parts Discussed in Thread: Z-STACK, MSP430F5438
Hi Friends,
I need to achieve security in zigbee communication.
I have done following settings for secure communication.
SECURE = 1,
zgPreConfigKeys = TRUE,
Default Key
I have following doubts.
1) If I set same settings in coordinator and end device, it would work well.
If I change the default key in ( f8wConfig.cfg )end device, end device would reset again and again with some interval time.
What is the reason for that?
2) I have set SECURE =0 in end device and SECURE = 1 in coordinator.
The end device was connected to coordinator but data transfer are not working.
How end device connected to coordinator?
Is it correct?
Regards,
Keerthi G