This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Z-Stack GW] no RX data with UART

Other Parts Discussed in Thread: Z-STACK, CC2530, CC2531

With Z-Stack Linux Gateway (v1.0.1), when calling server invoke script, servers did not bring up properly.

It seems that there is a problem with UART RX, but not sure about the cause.

At UART RX thread, there was no data read, ('readcound" always was "-1").

From H/W view point, the UART port worked well when connected with serial console of a PC.

However, when connected with CC2530 Development Kit, it sends Tx data via UART port, but Rx data, readcount always was "-1".

Can you guess what is the cause of the problem?

 

Thanks and regards,

Hayden